Skip to main content
JayDev
Senior
January 28, 2021
Question

Question with editing linker file (variable stored in flash)

  • January 28, 2021
  • 3 replies
  • 2341 views

Hello! I was trying to set aside a section in flash for a variable (I do have a reason to be doing so but, for the time being, I'm in the learning process to make sure I understand how it works before I do anything (too) stupid).

Anyway, my chip was the STM32L412RB. I am currently setting it up so I can set aside the last 16 bytes of flash for a variable location that I'm calling FLASH_ARRAY.

I managed to get it to recognize the last 16 bytes of flash for the variable, so that part looks good. Here is my code

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 40K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128k-16
 FLASH_VAR (rx) : ORIGIN = 0x801FFF0, LENGTH = 16
}

So far, all looks good and it's assigning the section 16 bytes in this section in the Memory Details section in STM32CubeIDE.

The problem comes when I'm trying to assign a specific location within this section (say I want to assign a specific variable inside this location, for instance). Below is effectively how I want to assign a variable, for instance (below is only one variable but, I could potentially add multiple variables in this section).

uint8_t flash_array[16]
__attribute__((section(".flash_var .FLASH_ARRAY")));

If I understand what I'm seeing on another example (as I'm seeing at this location: https://stackoverflow.com/questions/58256229/stm32f0-how-do-i-assign-values-from-variables-in-ram-to-a-separate-variable ), this can potentially be done with the following added to the "SECTIONS" section:

.flash_var :
 {
 KEEP(*(.flash_var .FLASH_ARRAY))
 *(.flash_var *);
 } > FLASH_VAR

When I try and run this though, I get the following errors:

section `.flash_var' will not fit in region `FLASH_VAR'
`FLASH_VAR' overflowed by 947837 bytes

Clearly, I set that last section up wrong, since the errors are introduced when I add that in. Since I don't seem to assign the variable a specific location (or size), I assume it's defaulting to a significantly larger size? I originally thought it might've been related to the min heap (0x200) or stack size (0x400) but that doesn't make sense in this context, from what I can see.

Could even be that I can't declare a section in flash smaller than a flash page size (which I need to look up, actually, that could be it). I found something regarding there being 64 pages of 2 kb programming. Does this mean I need to have sections that are all at least 2 kB? 64 pages of 2 kb would be 128 kb, so that does make sense . . .

EDIT: Ok, I tried the following and I'm getting the same errors, so I guess it's not that . . .

MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 40K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 126k
 FLASH_VAR (rx) : ORIGIN = 0x801E000, LENGTH = 2k
}

Any idea what might be going on here? I believe I'm close but I'm not quite there yet. Any info you can give me would be appreciated. Thanks!

This topic has been closed for replies.

3 replies

KnarfB
Super User
January 30, 2021

Try simpler names, not containing spaces " ". Like:

__attribute__((section(".flash_var.FLASH_ARRAY")));

KEEP(*(.flash_var.FLASH_ARRAY))

*(.flash_var*);

Actually, the names have no semantics that would matter. Also the KEEP only matters if you are *not* using your variable and still want it to be in the flash (like that version number info).

Otherwise, your code looks good.

hth

KnarfB

Associate III
June 22, 2023

Hello! Did you solve the issue? I got your same error

Tesla DeLorean
Guru
June 22, 2023

Show salient portion of code and whole error message rather than #metoo an older thread.

If you've overflowed a section, put less in it or figure why it is so large.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..