Skip to main content
Associate II
Aug 20, 2026 11:08 AM UTC
Solved

Question regarding interrupt and memory barriers

Hello, 

I have a kind of general question about the usage of interruptions and memory barriers.

Because of the pipeline architecture of the processor, it is recommanded by ARM (https://support.arm.com/documentation/dai0321/a/ ) to use DSB / ISB instruction when enabling disabling instruction. The guide focuses (amongst othr cases) on the NVIC operations. The CMSIS functions __NVIC_DisableIRQ and __NVIC_EnableIRQ look to respect the guidelines.

However, I’m wondering if such practices should be applied when enabling/disabling the peripheral interrupt (typically via the enable interrupt register) ? Same with the RegisterCallback functions avaialble in the HAl libraries.

 

Regards.

 

TDK
TDKBest answer
Aug 20, 2026 1:11 PM UTC

There’s no one size fits all rule here. In general, disabling or enabling interrupts does not necessitate a data or instruction barrier. You would only need one if you are doing something that requires the change to have taken effect. For example, you will see them prior to entering low-power modes for this reason.

"If you feel a post has answered your question, please click ""Accept as Solution""."

5 replies

TDK
TDKBest answer
Aug 20, 2026 1:11 PM UTC

There’s no one size fits all rule here. In general, disabling or enabling interrupts does not necessitate a data or instruction barrier. You would only need one if you are doing something that requires the change to have taken effect. For example, you will see them prior to entering low-power modes for this reason.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tahm_AAuthor
Associate II
Aug 20, 2026 2:14 PM UTC

What do you mean by “You would only need one if you are doing something that requires the change to have taken effect” ? Could you elaborate ?

TDK
Aug 20, 2026 3:09 PM UTC

I did elaborate with the low power example. What are you having trouble with?

"If you feel a post has answered your question, please click ""Accept as Solution""."