Skip to main content
Associate
Mar 19, 2026 8:38 AM UTC
Solved

Question on VDD and VSS internal connection

Should each vdd pin of the stm32f407zgt6 read continuity like the blue pill on multimeter, are they internally connected within the chip or separated? Similary for all the vss pins are they also all connected vss inside stm32f407zgt6

Thanks

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 19, 2026 9:32 AM UTC

You can't rely on the continuity test for that as not all VDD pins are internally connected together. Same case for VSS.

I've just tested it in a free chip.

Hope I answered your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

13 replies

mƎALLEm
ST Technical Moderator
Mar 19, 2026 8:52 AM UTC

Hello @OLAMIDESET and welcome to the ST community,

All VDD and VSS pins should be connected outside the chip (if this is the background of your question).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
Mar 19, 2026 9:00 AM UTC

I appreciate your prompt response. I know that all the vdd and vss pins should be connected and grounded with 100nf ceramic capacitor but what I'm saying is that before connecting any component at all, should each vdd pin read continuity on a multimeter and same thing with vss(are all vss internally grounded)?

mƎALLEm
ST Technical Moderator
Mar 19, 2026 9:04 AM UTC

@OLAMIDESET wrote:

should each vdd pin read continuity on a multimeter and same thing with vss(are all vss internally grounded)?


What is the background of that question? is that quiet important information to know?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.