Question
Question About USB device Lib
Posted on June 24, 2012 at 14:23
Hello
I'm working on USB device library V3.3.0; I'm new be in STM32 USB; I have some question:could you please help me 1/ I don't understand why SYSCFG module clock is used for the USB disconnect feature ? 2/ What GPIO_AINConfig() function do exactelly ? 3/ EXTERNAL_PULLUP and INTERNAL_PULLUP what are the differences and how they work ? 4/ PWR_EnterSTOPMode () is STM32 in STOP mode ? I measured IDD I get a high value around (2mA) 5/What Get_SerialNum(void) fuction do ?? Tanks Abdul Kalam