Skip to main content
qinghui
Visitor II
May 7, 2013
Question

Question about the RTC of STM32F103

  • May 7, 2013
  • 0 replies
  • 465 views
Posted on May 07, 2013 at 15:29

We're using RTC as a timer to wakeup STM32F103 from stop mode frequently, I'm quite confused on the descriptions in RM0008

1. what's the difference between RTC_IRQHandler and RTCAlarm_IRQHandler? If an alarm comes, both irq called? Is there a EXTI17_IRQHanlder?

2. do I must clear all of EXTI_Line17, PWR_FLAG_WU, RTC_IT_ALR in some irq handler? what's the actual physical connection between the components that these registers reside on (plz help to explain based on Figure 179 in RM0008)?

Thanks a lot!

#rtc #stm32f1
This topic has been closed for replies.