Question
Question about GPIO port defined as AF
Posted on December 04, 2012 at 19:17
I noticed on the STM3210E-EVAL board design and in the demo code GPIO port A was defined as AF for SPI1 and for USART. The chip select pin for the SPI flash memory was defined as pin 2 in GPIO port B. Does it mean once port A is defined as AF, all the pins have to be AF? Can I define Port A poin 4 as SPI flash chip select?