Skip to main content
pcu
Associate III
Oct 2, 2014 3:05 PM UTC
Question

Question about external RAM and SD

Posted on October 02, 2014 at 17:05

Hello,

I try to test my application with a new setup with external SRAM on the STM3240G kit, for heap and stack.

I use FatFS on SDIO which needs DMA. When I read a file there is a problem.

I know it is not possible to read a file to CCMRAM because of the DMA. Then is it the same problem?

Thank you.
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    Oct 2, 2014 4:04 PM UTC
    Posted on October 02, 2014 at 18:04

    You should be able to DMA to external memory (FSMC), but it will be slower, with whatever ramifications come with that. ie 16-bit wide, multiple cycles, heavier contention.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    pcu
    pcuAuthor
    Associate III
    Oct 3, 2014 9:37 AM UTC
    Posted on October 03, 2014 at 11:37

    Of course, it will be slower. But if I don't have enough memory I must see for alternate solution.

    I will check why I can't access the SD with variables(stack memory) stored on external SRAM

    .

    KR.

    frankmeyer9
    Associate III
    Oct 3, 2014 9:49 AM UTC
    Posted on October 03, 2014 at 11:49

    Of course, it will be slower.

     

    There are two thing to mention here:

    First, you cannot startup with an external stack, as it does not exist at this stage.

    Second, if you have a rigid interrupt regime, it might blow. Interrupts imply stack operations.

    I would opt for other data to move to external RAM, but not the stack.

    But if I don't have enough memory I must see for alternate solution.

     

    There are other MCUs, and other vendors.