QUADSPI + DMA, reading too many bytes?
Hello, so I am trying to write a driver for a GigaDevice GD5F2GQ4xFxxG part, that uses the QUADSPI peripheral. So far so good, but seeing some unexpected results and when I dug into it, I think I observe that a read command is acquiring more bytes than I expect.
Specifically, the code below is called with a parameter count_of_bytes_to_transfer equal to 18, but in the destination array, I think I see that 23 bytes are actually being set... the first 18 correctly, then the next five to random values (possibly unset bytes in the FLASH).
This is my first time using QUADSPI, and I have only utilized DMA a handful of times, so I worked out the code by trial and error. I set *both* the QUADSPI->DLR and DMA->CNDTR registers to the appropriate lengths (N-1 and N, respectively, which is what the ref manual says they want), but wasn't sure I needed to set both, or which one was correct. Anyway, this doesn't explain why I could possibly be clocking out *23* bytes with this code.
Could this have to do with my misunderstanding of the interaction between QUADSPI and DMA? I'm imagining that maybe my FIFO empties out for some reason, after CNDTR and DNR are decremented to zero.
Also, my code determines that the read is complete by looking for the DMA TCIF interrupt, and then disables DMA using DMA1_Channel5->CCR &= ~(1<<0). I patterned this after some sample code I found... it seemed to work fine. But now I've noticed this overrun and I'm reconsidering things.
Anyway, does anyone have a theory as to why I'm reading more bytes than expected, or notice anything I'm doing wrong with my described approach?
Thanks very much for any help, STM32 geniuses.
static void StartTransfer_0xEBReadFromCacheQuad(uint16_t source_column_address, uint8_t * local_target, uint16_t count_of_bytes_to_transfer)
{
//////////////////////////////////////////////////////////////////////////
// activate DMA
//////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////
// 0xEB Read from cache quad IO
//
// Instruction phase: yes, one line, 0xEB
// Address phase: yes, four lines, two bytes of column address
// Alternate-bytes phase: no
// Dummy-cycles phase: yes, two cycles (for one byte in quad mode)
// Data phase: yes, four lines
//
// notes: 1) "column address" is the byte within the page, 0-2175 when ECC
// disabled, 0-2111 when ECC enabled
// 2) since this is a read but requires an address, will be triggered
// by writing to the address register
//
//////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////
// Set QUADSPI CCR [RM0394, 15.5.6]
//////////////////////////////////////////////////////////////////////////
// 33222222222211111111110000000000
// 10987654321098765432109876543210
// --------------------------------
QUADSPI->CCR = 0x07081DEB; // = 00000111000010000001110111101011
// || | | | | | | | | | |
// || | | | | | | | | | +--- 7:0 INSTRUCTION = 11101011 = 0xeb Instruction = 0xEB
// || | | | | | | | | +----------- 9:8 IMODE = 01 = 0x1 Instruction on a single line
// || | | | | | | | +------------- 11:10 ADMODE = 11 = 0x3 Address on four lines
// || | | | | | | +--------------- 13:12 ADSIZE = 01 = 0x1 16-bit address
// || | | | | | +----------------- 15:14 ABMODE = 00 = 0x0 No alternate bytes
// || | | | | +------------------- 17:16 ABSIZE = 00 = 0x0 8-bit alternate byte
// || | | | +--------------------- 22:18 DCYC = 00010 = 0x2 2 dummy cycles
// || | | +--------------------------- 25:24 DMODE = 11 = 0x3 Data on four lines
// || | +----------------------------- 27:26 FMODE = 01 = 0x1 Indirect read mode.
// || +------------------------------- 28:28 SIOO = 0 = 0x0 Send instruction on every transaction.
// |+--------------------------------- 30:30 DHHC = 0 = 0x0 Delay the data output using analog delay
// +---------------------------------- 31:31 DDRM = 0 = 0x0 DDR Mode disabled
QUADSPI->DLR = count_of_bytes_to_transfer - 1;
//////////////////////////////////////////////////////////////////////////
// setting the address will trigger the transfer
//////////////////////////////////////////////////////////////////////////
QUADSPI->AR = source_column_address;
//////////////////////////////////////////////////////////////////////////
// set the peripheral address to QuadSPI data register
// set the memory address to the specified location
// set the count to be moved;
// The data is moved from this address to the memory after the peripheral event
//////////////////////////////////////////////////////////////////////////
uint32_t address_of_QUADSPI_DR = (uint32_t) &(QUADSPI->DR);
DMA1_Channel5->CPAR = address_of_QUADSPI_DR; // QUADSPI->DR;
DMA1_Channel5->CMAR = (uint32_t) local_target;
DMA1_Channel5->CNDTR = count_of_bytes_to_transfer;
//////////////////////////////////////////////////////////////////////////
// Set DMA1 CCR5 [RM0394, 11.6.3]
//////////////////////////////////////////////////////////////////////////
// 33222222222211111111110000000000
// 10987654321098765432109876543210
// --------------------------------
DMA1_Channel5->CCR = 0x0000308B; // = 00000000000000000011000010001011
// | | | |||||||||
// | | | ||||||||+--- 0:0 EN = 1 = 0x1 DMA channel enabled
// | | | |||||||+---- 1:1 TCIE = 1 = 0x1 transfer complete interrupt (TCI) enabled
// | | | ||||||+----- 2:2 HTIE = 0 = 0x0 half transfer interrupt (HTI) disabled
// | | | |||||+------ 3:3 TEIE = 1 = 0x1 transfer error interrupt (TEI) enabled
// | | | ||||+------- 4:4 DIR = 0 = 0x0 data transfer reads from peripheral
// | | | |||+-------- 5:5 CIRC = 0 = 0x0 circular mode disabled
// | | | ||+--------- 6:6 PINC = 0 = 0x0 peripheral increment mode disabled
// | | | |+---------- 7:7 MINC = 1 = 0x1 memory increment mode enabled
// | | | +----------- 9:8 PSIZE = 00 = 0x0 peripheral size is 8 bits
// | | +------------- 11:10 MSIZE = 00 = 0x0 memory size is 8 bits
// | +--------------- 13:12 PL = 11 = 0x3 priority level very high
// +----------------- 14:14 MEM2MEM = 0 = 0x0 memory-to-memory disabled
}