Skip to main content
Associate III
Sep 24, 2017 10:31 AM UTC
Question

quad SPI to SPI DMA

Posted on September 24, 2017 at 12:31

Hello,

I have a data in stored in quad SPI memory on device A, that I want to transmit to device B using SPI interface.

I was wondering if its possible to steam directly from quad-spi memory to SPI interface using DMA without buffering?

I have STM32L476 Discovery for testing

Thanks

Michael

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    Sep 24, 2017 10:38 AM UTC
    Posted on September 24, 2017 at 12:38

    Never tried, but I'd say yes, if the QSPI is in memory-mapped mode and the DMA is triggered from the SPI, it should behave as any other memory-to-SPI DMA. I wouldn't count on continuous SPI clock in case of SPI being master, though, and would consider timing issues should the SPI be slave.

    JW

    privenAuthor
    Associate III
    Sep 25, 2017 1:17 PM UTC
    Posted on September 25, 2017 at 13:17

    JW,

    Thank you for your replay, its a good idea to use QSPI and memory mapped.

    The SPI is slave, how can I evaluate the timing and check for issues?

    Michael