Skip to main content
cVass.1
Associate II
November 7, 2020
Question

Qspi stm32h743

  • November 7, 2020
  • 8 replies
  • 2126 views

​Hello.

I am looking for example of External Qspi Loader for the Stm32h743.

I manage to make my functions work. but not to create the .stldr

I have the impression that he does not take Init.

I am under Stm32cubeide.

thank you

This topic has been closed for replies.

8 replies

Bowman32
ST Employee
November 9, 2020

Hi @cVass.1​ 

You can refer to available QSPI examples with STM32CubeH7 firmware: STM32Cube_FW_H7_V1.6.0\Projects\STM32H743I-EVAL\Examples\QSPI

Bouraoui

cVass.1
cVass.1Author
Associate II
November 10, 2020

thank you,

but no example to create an External Loader.

On my tests I must do a Disconnect and Connect to manage to put in Mapping.

Bowman32
ST Employee
November 11, 2020

Hi @cVass.1​ 

You can refer to application note "Quad-SPI interface on STM32 microcontrollers and microprocessors" AN4760 

Bouraoui

cVass.1
cVass.1Author
Associate II
November 13, 2020

hello, whatever progress a Read gives me an error message.

Here I do a Disconnect then a Connect, it works

Do you have an idea

thank you

YGU.1
Associate II
November 26, 2020

Hi cVass.1

I'm struggling with the same problem. I've created required functions, tested them in the stm32cubeide and everything looks OK. I managed read and write an external flash (1M). Then I added Loader_Src.c and Dev_Inf to the project and built it with the linker (please find attachment). I got .stldr and copied it to the appropriate folder of the STM32CubeProgrammer. Now I can read the external flash by STM32CubeProgrammer, but unfortunatelly cannot erase and write. The error message says: failed to erase memory... Please let me know if you have some progress.

Thanks

cVass.1
cVass.1Author
Associate II
November 26, 2020

hello can you send me the complete project. Thank you

cVass.1
cVass.1Author
Associate II
November 26, 2020

Hello

my Linker is identical

can you show me my Loader_Src and Dev_Inf.

Thank you

Bowman32
ST Employee
December 14, 2020

Hi @cVass.1​ 

Can you share your project and the target memory's datasheet?

Bouraoui