Skip to main content
Associate III
October 1, 2024
Question

QSPI NOR Flash: can write data but can't read from it

Hi 

i am using stm32f767IGK6 i am able to write data in nor flash but  can't read  data of same address.

by use this APIs HAL_QSPI_Transmit(), HAL_QSPI_Receive()

 

Regard & Thanks,

Naresh 

This topic has been closed for replies.

3 replies

KDJEM.1
ST Technical Moderator
October 1, 2024

Hello @Naresh_ ,

 

Could you please give more detail about the issue.

Are you read data in memory mapped mode or indirect mode?

Could you please take a look at the errata sheet precisely:

  • 2.4.2 Wrong data from memory-mapped read after an indirect mode operation
  • 2.4.4 Memory-mapped access in indirect mode clearing QUADSPI_AR register

May QSPI_ReadWrite_IT this example can help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
October 1, 2024

Your presentation of the problem and the context is inadequate.  Try harder as if you're explaining to someone who's not physically watching you code and test the issue.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Naresh_Author
Associate III
October 16, 2024

Hi ,

Now i am able to Read  Manufacturer ID and the Device ID Nor flash by using below code 

 

 

s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;

 s_command.Instruction = S25FL128S_READ_ID_CMD;//0x90 or 0x9f

 s_command.Address = QSPI_ADDRESS_NONE;

 s_command.AddressMode = QSPI_ADDRESS_NONE;

 s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

 s_command.DataMode = QSPI_DATA_1_LINE;

 s_command.NbData = 3;

 s_command.DummyCycles = 0;

 s_command.DdrMode = QSPI_DDR_MODE_DISABLE;

 s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;



/* Configure the command */

if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

return S25FL128S_ERROR;

 }

/* Reception of the data */

if (HAL_QSPI_Receive(Ctx, ID, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

return S25FL128S_ERROR;

 }

 

  when i am trying read nor flash then based data lines it change data like 255, 81.. as below showing code 

 

 

s_command.AddressSize = QSPI_ADDRESS_32_BITS;
	 s_command.Address = ReadAddr;
	 s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
	 s_command.NbData = Size;
	 s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
	 s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

	 /* Configure the command */
	 if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
	 {
	 return S25FL128S_ERROR;
	 }

	 /* Reception of the data */
	 if (HAL_QSPI_Receive(Ctx, pData, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
	 {
	 return S25FL128S_ERROR;
}

 

when i trying to write enable and  write then it is not working can please help 

i send instruction is 0x6 for write enable then it send error at this API's is HAL_QSPI_AutoPolling() time issue

 

QSPI_CommandTypeDef s_command;
 QSPI_AutoPollingTypeDef s_config;

 UNUSED(Mode); /* The command Write Enable is always 1-0-0 */

 /* Enable write operations */
 s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
 s_command.Instruction = S25FL128S_WRITE_ENABLE_CMD;
 s_command.Address = QSPI_ADDRESS_NONE;
 s_command.AddressMode = QSPI_ADDRESS_NONE;
 s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
 s_command.DataMode = QSPI_DATA_1_LINE; // changed to 0 data to l data line
 s_command.DummyCycles = 0;
 s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
 s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

 if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 return S25FL128S_ERROR;
 }

 /* Configure automatic polling mode to wait for write enabling */
 s_config.Match = S25FL128S_SR1_WREN;
 s_config.Mask = S25FL128S_SR1_WREN;
 //s_config.MatchMode = QSPI_MATCH_MODE_AND;
 s_config.MatchMode = QSPI_MATCH_MODE_OR;
 s_config.StatusBytesSize = 1;
 //s_config.Interval = 0x10;
 s_config.Interval = 0xFF;
 s_config.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
 s_command.Instruction = S25FL128S_READ_STATUS_REG1_CMD;
 s_command.DataMode = QSPI_DATA_1_LINE;

 if (HAL_QSPI_AutoPolling(Ctx, &s_command, &s_config, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 return S25FL128S_ERROR;
 }




HAL_StatusTypeDef HAL_QSPI_AutoPolling(QSPI_HandleTypeDef *hqspi, QSPI_CommandTypeDef *cmd, QSPI_AutoPollingTypeDef *cfg, uint32_t Timeout)
{
 HAL_StatusTypeDef status;
 uint32_t tickstart = HAL_GetTick();

 /* Check the parameters */
 assert_param(IS_QSPI_INSTRUCTION_MODE(cmd->InstructionMode));
 if (cmd->InstructionMode != QSPI_INSTRUCTION_NONE)
 {
 assert_param(IS_QSPI_INSTRUCTION(cmd->Instruction));
 }

 assert_param(IS_QSPI_ADDRESS_MODE(cmd->AddressMode));
 if (cmd->AddressMode != QSPI_ADDRESS_NONE)
 {
 assert_param(IS_QSPI_ADDRESS_SIZE(cmd->AddressSize));
 }

 assert_param(IS_QSPI_ALTERNATE_BYTES_MODE(cmd->AlternateByteMode));
 if (cmd->AlternateByteMode != QSPI_ALTERNATE_BYTES_NONE)
 {
 assert_param(IS_QSPI_ALTERNATE_BYTES_SIZE(cmd->AlternateBytesSize));
 }

 assert_param(IS_QSPI_DUMMY_CYCLES(cmd->DummyCycles));
 assert_param(IS_QSPI_DATA_MODE(cmd->DataMode));

 assert_param(IS_QSPI_DDR_MODE(cmd->DdrMode));
 assert_param(IS_QSPI_DDR_HHC(cmd->DdrHoldHalfCycle));
 assert_param(IS_QSPI_SIOO_MODE(cmd->SIOOMode));

 assert_param(IS_QSPI_INTERVAL(cfg->Interval));
 assert_param(IS_QSPI_STATUS_BYTES_SIZE(cfg->StatusBytesSize));
 assert_param(IS_QSPI_MATCH_MODE(cfg->MatchMode));

 /* Process locked */
 __HAL_LOCK(hqspi);

 if(hqspi->State == HAL_QSPI_STATE_READY)
 {
 hqspi->ErrorCode = HAL_QSPI_ERROR_NONE;

 /* Update state */
 hqspi->State = HAL_QSPI_STATE_BUSY_AUTO_POLLING;

 /* Wait till BUSY flag reset */
 status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_BUSY, RESET, tickstart, Timeout);

 if (status == HAL_OK)
 {
 /* Configure QSPI: PSMAR register with the status match value */
 WRITE_REG(hqspi->Instance->PSMAR, cfg->Match);

 /* Configure QSPI: PSMKR register with the status mask value */
 WRITE_REG(hqspi->Instance->PSMKR, cfg->Mask);

 /* Configure QSPI: PIR register with the interval value */
 WRITE_REG(hqspi->Instance->PIR, cfg->Interval);

 /* Configure QSPI: CR register with Match mode and Automatic stop enabled
 (otherwise there will be an infinite loop in blocking mode) */
 MODIFY_REG(hqspi->Instance->CR, (QUADSPI_CR_PMM | QUADSPI_CR_APMS),
 (cfg->MatchMode | QSPI_AUTOMATIC_STOP_ENABLE));

 /* Call the configuration function */
 cmd->NbData = cfg->StatusBytesSize;
 QSPI_Config(hqspi, cmd, QSPI_FUNCTIONAL_MODE_AUTO_POLLING);

 /* Wait until SM flag is set to go back in idle state ***** */
 status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_SM, SET, tickstart, Timeout);

 if (status == HAL_OK)
 {
 __HAL_QSPI_CLEAR_FLAG(hqspi, QSPI_FLAG_SM);

 /* Update state */
 hqspi->State = HAL_QSPI_STATE_READY;
 }
 }
 }
 else
 {
 status = HAL_BUSY;
 }

 /* Process unlocked */
 __HAL_UNLOCK(hqspi);

 /* Return function status */
 return status;
}

 

status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_SM, SET, tickstart, Timeout); i am fail to check the status register of nor flash. 

 

how to do write_enable , write operation in nor flash?

 

Regards & Thanks,

Naresh