QSPI Configuration using SST26VF032B-104I
Hi STM,
I have some questions for QSPI configuration using SST26VF032B-104I (Max clock = 104 MHz)
I am getting QSPI_SUSPENDED Error when I call BSP_QSPI_GetStatus().
Configuration is as follow;
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
QSPIHandle.Init.ClockPrescaler = 2; /* QSPI freq = 216 MHz/(1+2) = 72 Mhz */
QSPIHandle.Init.FifoThreshold = 4; QSPIHandle.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE; QSPIHandle.Init.FlashSize = POSITION_VAL(SST26VF032B_FLASH_SIZE) - 1; QSPIHandle.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_2_CYCLE; /* Min 30ns for nonRead */ QSPIHandle.Init.ClockMode = QSPI_CLOCK_MODE_0; QSPIHandle.Init.FlashID = QSPI_FLASH_ID_1; QSPIHandle.Init.DualFlash = QSPI_DUALFLASH_DISABLE;//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
I don't know what is wrong.
Please advise me.
Thanks.
Regards,
Thiha Kyaw