Question
QSPI bank2 <-> s/f memory is possible?
Hello,
I have question about QSPI on stm32F446.
I want to connect serial flash with QSPI.
there are 2 banks on QSPI.
When I try to find some example on QSPI, they were all used QSPI bank1 connected to s/f memory.
But when I check pin connections on QSPI bk1 style, pins are spread all over the chip. seems not good. But QSPI with bk2 is get together except cs pin, but looks very nice. So I want to use QSPI with bk2, Is is possible? And What is bk2's address?
Thanks for reading.
Best Regards,
Tiel.