PWM TIM3
Hi,
I am using STM32 F303 VCT6 and want to output PWM signal on TIM3, TIM2.
I followed the instructions in some video to build the code using STM32CubeMX.
I set the Clock Source for both timers to 'Internal Clock'.
I set all four channels for bother timers to 'PWM Generation Chx'
I set the Parameter Settings as follows:
Prescaler: 16
Counter Period (AutoReload Register): 100
Pulse: different values to each channel from 25 to 100
I created the project and then started the timers:
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1); // for each channel and for both timers.
The question is, what is still missing? I dont get any output on the timers????