Question
PWM Output on STM3210E-EVAL board
Posted on August 27, 2015 at 23:11
I'm trying to setup one of the LEDs on the STM3210E-EVAL board as a PWM output so that I can vary the brightness. I am targeting the red LED, which is on port F, pin 8. I have setup timer 13 which should be tied to that pin for PWM output, but I feel like like I am missing a step somewhere. Here is the current function to initialize the pin, setup the timer, and setup the PWM:
void led_init(void)
{
TIM_OC_InitTypeDef sConfigOC;
TIM_HandleTypeDef htim13;
/*Configure GPIO pins : PF8 */
__HAL_AFIO_REMAP_TIM13_ENABLE();
__GPIOF_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
htimInstance = TIM13;
htimInit.Prescaler = (uint32_t)(72000000 / 2000000) - 1;
htimInit.CounterMode = TIM_COUNTERMODE_UP;
htimInit.Period = 700;
htimInit.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_Base_Init(&htim13);
HAL_TIM_PWM_Init(&htim13);
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 350;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
HAL_TIM_PWM_ConfigChannel(&htim13, &sConfigOC, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim13, TIM_CHANNEL_1);
}
Any advice would be greatly appreciated!
Thank you!
#stm32f103 #stm3120e-eval