Skip to main content
Associate III
Nov 18, 2025 9:47 AM UTC
Question

PWM jitter on a home made card

Hello everyone,

 

Some time ago I asked on this website information about jitter on a PWM : Solved: PWM jitter - STMicroelectronics Community

The problem was that when generating a PWM, it wasn't very stable. At the time changing the source clock to the external clock of the nucleoboard worked and stabilized everything.

Since then, I created my own board using an STM32G474QE (128 pins) with an 8MHz (+/-50ppm) external oscillator.

I tried to generate the PWM and I am encountering the same exact problem again, the jitter is back. This time, I directly setup the clock as the external one. 

I checked it up and it feels to me that the problem could be coming from the stability of my oscillator (I have frequency variation on it's output ranging from 7,999,950 to 8,000,050Hz). 

Now my question is, could this really be the problem and could a lower ppm oscillator work ?

I tried looking up information on my own especially using AN2867 but I only get information about crystal oscillator.

Thank you very much for any answer provided

 

9 replies

Andrew Neil
Super User
Nov 18, 2025 9:53 AM UTC

Please show your schematic and some good, clear photographs of your board & setup

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EliazLBAuthor
Associate III
Nov 18, 2025 10:14 AM UTC

Here is the schematic and a picture of the µcontroller. The 8Mhz oscillator is the smaller one on the right.

The part is 831072801.

mƎALLEm
ST Technical Moderator
Nov 18, 2025 10:36 AM UTC

Hello,

Are you sure you selected HSE as the source clock for the PLL?

mALLEm_1-1763462193851.png

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
EliazLBAuthor
Associate III
Nov 18, 2025 10:53 AM UTC

Yes, this is my configuration for the clock

AScha.3
Super User
Nov 18, 2025 1:44 PM UTC

Hi,

the jitter from your oszillator 831072801  is about: 

Period Jitter (pk-pk): ±80ps typ , you might not see on any scope.

 

So check at first using the 8MHz input direct, not with PLL in the clock tree. (should give some  ±10ps typ ).

Then try same, but with PLL -> high frequency ; and do not use extreme PLL settings (low or very high frequency output) , because the PLLs have a range of input and output frequencies, they are optimized for.

Maybe check in ds of your cpu, might have some jitter data for the PLL driven clocks, from ds G474 :

AScha3_0-1763473255748.png

So the PLL is not as good as without PLL (10ps -> 21 ps) , but not visible on a scope.

 

 

If you feel a post has answered your question, please click on " Best Answer ".
EliazLBAuthor
Associate III
Nov 18, 2025 2:35 PM UTC

I have tried both but it doesn't seem to change much.