Skip to main content
adamajames2
Associate II
September 2, 2008
Question

PWM In and Out using same Timer problem

  • September 2, 2008
  • 1 reply
  • 460 views
Posted on September 02, 2008 at 07:32

PWM In and Out using same Timer problem

    This topic has been closed for replies.

    1 reply

    adamajames2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:43

    Hello,

    I was/am trying to generate a PWM signal (41KHz) using Timer 2 channel 3 (PWM1) and then for testing read back the signal on channel 2 (PWMI). However the frequency I read using TIM_GetCapture2(TIM2) is always incorrect (it just reads 4). The Duty Cycle I read using TIM_GetCapture1(TIM2) is correct.

    I have tried doing all of this using Timer 3 and get the same frequency issue and I've tried different frequencies for the output wave.

    I have so far had to use Timer 2 to generate the signal and Timer 3 to read the signal and this works without problem, but does use an extra timer, which i'll probably need later.

    Should it be possible? Am I doing something wrong?

    Adam