Skip to main content
kisaravanan
Visitor II
April 18, 2013
Question

PVD through EXTI Line detection not triggered!

  • April 18, 2013
  • 4 replies
  • 1152 views
Posted on April 18, 2013 at 09:29

Hi

In STM32F103RC, Configured the interrupt for PVD through EXTI line 16,

When the PVDO output bit is on in PWR_CR, but interrupt not triggerd!

Thanks

#pvdo-interrupt
This topic has been closed for replies.

4 replies

Amel NASRI
ST Technical Moderator
May 9, 2013
Posted on May 09, 2013 at 15:45

Hello,

Try to share some code for check. Did you tried different voltage thresholds?

Regards,

ST.MCU

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
jpeacock2399
Associate III
May 10, 2013
Posted on May 11, 2013 at 01:01

// Enable the EXTI16 (PVD) Power Supervisor Interrupt 
// EXTI16 rising edge for falling voltage, falling edge for rising voltage on PVD 
#if (CPUID_PARTNO == CPUID_CORTEX_M3 && CPUID_VARIANT == 0) // for STM32F1xx 
PWR_PVDLevelConfig(PWR_PVDLevel_2V9); // 2.9V falling to trigger powerfail 
#else 
PWR_PVDLevelConfig(PWR_PVDLevel_7); // 2.9V falling to trigger powerfail 
#endif 
PWR_PVDCmd(ENABLE); // enable PVD 
NVIC_InitStructure.NVIC_IRQChannel = PVD_IRQn; // PVD programmable voltage detect 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = BKPDEV_PVD_PRIORITY; 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
NVIC_Init(&NVIC_InitStructure); 
EXTI_ClearITPendingBit(EXTI_Line16); // clear pending IRQs 
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; 
EXTI_InitStructure.EXTI_Line = EXTI_Line16; // set up irq trigger 
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; // trigger power rising edge (voltage drop) 
EXTI_InitStructure.EXTI_LineCmd = ENABLE; // alert if power status changes 
EXTI_Init(&EXTI_InitStructure);

This ishow I do it on F1/F2/F4. Jack Peacock
zexx86
Associate III
May 11, 2014
Posted on May 11, 2014 at 12:47

Hello

Did you found where is a problem?

I have same issue with 103RBT6, same code as above.

I can't even get any success with:

if ((PWR->CSR & PWR_FLAG_PVDO) != (uint32_t)RESET)

Thanks
zexx86
Associate III
May 11, 2014
Posted on May 12, 2014 at 00:15

Problem solved. With source code from PVD example it just works.

Thanks