Skip to main content
john doe
Senior III
January 17, 2017
Question

Proper way to use Cube_FW_ templates?

  • January 17, 2017
  • 2 replies
  • 572 views
Posted on January 17, 2017 at 05:21

How am I supposed to use these? I'm using SW32STM Workbench and can build projects from STM32CubeMX-generated code. I can build and run code from the Cube_FW_Fx examples.

But when I try to copy the files from the Templates into a new directory then import it, it takes some hand-waving to add all the includes, and even then, it complains of a missing target.

Building file: /Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s

Invoking: MCU GCC Assembler

/Users/john/src/stm32/stm32f7xx/templt/SW4STM32/STM32F769I_DISCOVERY_AXIM-FLASH/Debug

arm-none-eabi-as -mcpu=cortex-m7 -mthumb -mfloat-abi=hard -mfpu=fpv5-sp-d16 -g -o 'Example/SW4STM32/startup_stm32f769xx.o' '/Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s'

Finished building: /Users/john/src/stm32/stm32f7xx/templt/SW4STM32/startup_stm32f769xx.s

 

make: *** No rule to make target `/Users/john/src/Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.c', needed by `Drivers/STM32F7xx_HAL_Driver/stm32f7xx_hal.o'.  Stop.

21:25:23 Build Finished (took 2s.702ms)

I'm doing something improperly and I am not sure what. Goal is a template that includes BSP and syscalls.c Please advise.

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    January 17, 2017
    Posted on January 17, 2017 at 11:11

    Hello

    doe.john.016

    ,

    You can refer to this thread it will hep you on

    https://community.st.com/0D50X00009XkeN3SAJ

    .

    In the STM32CubeF7 firmware package, you may find pre-configured projects for the SW4STM32IDE as well as a template project.

    You may use them as a start pointto have more idea on how configuration/implementation is done.

    Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    john doe
    john doeAuthor
    Senior III
    January 17, 2017
    Posted on January 17, 2017 at 12:42

    The templates only work when I use them in place with their original name. How do I copy the template into a different filename and still get everything to resolve?