Skip to main content
GChen.6
Associate
April 27, 2020
Question

Proper method to know function under interrupt

  • April 27, 2020
  • 3 replies
  • 2284 views

Hi,

Currently, I am looking for the method to detect this function is under ISR or not.

And I found that there has two snipset code,

<Example 1>

uint8_t isUnderInterrupt(void)

{

uint8_t status = THREAD_MODE;

if (SCB->ICSR & SCB_ICSR_VECTACTIVE_Msk)

  {

     status = ISR_MODE;

  }

return status;

}

After I studying programming manual, I think above function is proper method to detect

this function is under ISR or not (If there has wrong thought, please correct me, thank you).

And I check some web example, someone uses freeRTOS with M3 MCU and the Example 2 using different way to implement it, but even I check programming manual, I cannot understand it,

<Example 2>

if (0 == __get_CONTROL())

{

// Under ISR

}

else

{

// Under Normal

}

How can using read out CONTROL register bit (SPSEL, nPRIV) to know MCU is under ISR? (M3 with freeRTOS).

By the way, if Example 2 is good method to know, when I use M4 MCU with FPU, the CONTROL register bit is (FPCA, SPSEL, nPRIV) the Example 2 is still work?

Please to give me some suggestion to guide me which method is proper one when using in M4 with FPU under freeRTOS, thank you so much.

    This topic has been closed for replies.

    3 replies

    Pavel A.
    April 27, 2020

    If you use FreeRTOS, just call xPortIsInsideInterrupt.

    "Some web example" is not a reliable source ;)

    -- pa

    TDK
    April 27, 2020

    The currently executing interrupt, if any, is stored in the VECTACTIVE bits in SCB->ICSR. This is a cortex register, look there for the details.

    // return true if we're in an interrupt
    inline bool InInterrupt() {
     return SCB->ICSR & SCB_ICSR_VECTACTIVE_Msk;
    }

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    GChen.6
    GChen.6Author
    Associate
    May 11, 2020

    Hi,

    Thank you all~~~

    All your suggestion is very useful : )