Skip to main content
marouenebrikcha
Associate II
March 19, 2012
Question

Programming keypad 4x4 using encoder 16 key on STM32VL

  • March 19, 2012
  • 6 replies
  • 1394 views
Posted on March 19, 2012 at 14:01

Heelo

I' using microcontroller STM32VL Discovery and i won't to interface caracter of keypad 16 key on LCD using an encoder 16 keys .

Please help me friend's !! 
    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    March 19, 2012
    Posted on March 19, 2012 at 15:09

    Wouldn't you just hook up the row/column to GPIO pins and scan it like every other implementation?

    A quick Google should manifest a whole slew of examples

    http://www.atmel.com/Images/doc2669.pdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    emalund
    Associate III
    March 19, 2012
    Posted on March 19, 2012 at 15:44

    I almost made a boo-boo once by routinely making the outputs to the keypad push-pull. That would make beautiful blue smoke come out of the chip if you press two keys at the same time. Fortunately, I caught it before loading the code into the micro.

    I can see someone making the same mistake by routine, thus this post.

    Erik

    emalund
    Associate III
    March 19, 2012
    Posted on March 19, 2012 at 15:51

    WOW, just had a peek at your Arghmel link and, lo and behold, they make that very mistake:

     ''Rows are connected to four PIO pins configured as outputs.''

    Erik

    emalund
    Associate III
    March 19, 2012
    Posted on March 19, 2012 at 15:51

    WOW, just had a peek at your Arghmel link and, lo and behold, they make that very mistake:

     ''Rows are connected to four PIO pins configured as outputs.''

    Erik

    marouenebrikcha
    Associate II
    March 19, 2012
    Posted on March 19, 2012 at 22:26

    marouenebrikcha
    Associate II
    March 19, 2012
    Posted on March 19, 2012 at 22:29