Skip to main content
mariemzidi
Associate II
March 4, 2010
Question

Programming an LCD via ST32F103ZE microcontroller

  • March 4, 2010
  • 13 replies
  • 2043 views
Posted on March 04, 2010 at 10:38

Programming an LCD via ST32F103ZE microcontroller

    This topic has been closed for replies.

    13 replies

    tkjmail2
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:42

    Hi.

    I've made a software application which takes a BMP and convert it into a hexadecimal byte array (char)

    Then I've made this function which shows the BMP;

    void DispPic(u16 x0, u16 y0, const unsigned char *str); 

    If you are interested I can send the code to you - OBS: the software is made in Visual Basic .NET!

    Best Regards

    Thomas Jespersen

    tkjmail2
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:42

    Of course.

    But as my other thread about a Hard Fault error explains, the code doesn't work probably. The code works on a STM32F103RET6, but on the STM32F103ZET6 it makes a Hard Fault error!

    Here is the thread:

    [DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/Hard Fault error&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%2520CortexM3%2520STM32/AllItems.aspx&currentviews=51]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fHard%20Fault%20error&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FARM%2520CortexM3%2520STM32%2FAllItems%2Easpx&currentviews=51

    But I will post the code when I have found and fixed the error!

    Best Regards

    Thomas Jespersen

    mariemzidi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:42

    Hi Thomas,

    I am really interested on the code (for displaying the BMP picture) you talked about..

    I will be very thankful if u send me the code..

    Best Regards,