Skip to main content
stock239955_stm1
Visitor II
September 21, 2012
Question

Programing STM32F407 with the STM32VLDISCOVERY using SWD interface

  • September 21, 2012
  • 1 reply
  • 663 views
Posted on September 21, 2012 at 23:26

Hi,

I'm trying to use the ST-Link on the STM32VLDISCOVERY board to program

a

STM32F407ZGT6

using the SWD interface but it just don't work ...

I'm getting the ''No target connect'' error. I have triple checked all the connections,

the board is properly powered, ST-link drivers and Utility are the latest versions

(with support to the Z batch of the STM32F4).

I have used this same setup (St-Link on the STM32VLDISCOVERY) to successfully

program STM32F1 MCUs ... is there any technical reason for the ST link on the

STM32VLDISCOVERY not to recognise the STM32F407ZGT6 ?

Best regards,

P

A

    This topic has been closed for replies.

    1 reply

    frankmeyer9
    Associate III
    September 22, 2012
    Posted on September 22, 2012 at 14:58

    I'm not sure if you can get this to work at all.

    But I'm not surprised it doesn't work out of the box. The VLDiscovery is the old V1 version of the STLink, which is rather messed up, by the way.

    There was no F4 released when the firmware for the VLDiscovery-STLink part was finalized. So no wonder it does not recognize the controller.

    You might fetch the STLink Utility software and try to update the STLink part. That worked for me with V2 (STM32F0_Discovery).

    But as said, I'm not sure about V1, never even tried that.