Skip to main content
Senior
June 14, 2024
Question

Program update

Hi,

1. is there any tool (GUI) to update program using executable?

2. How to have different modes of programming? (UART/ USB/ sd card)

3. Bootloader mentions: USB OTG FS (PA11/12) in Device mode (DFU: device firmware upgrade). Can external HS phy in FS as a device be used to update program?

 

This topic has been closed for replies.

16 replies

GauravKAuthor
Senior
June 26, 2024

questions: 1. is the .elf ok, I haven't changed anything to have different file

2. is boot1 pin changes needed?

3. Is any change if CubeProgrammer needed for PID, VID for USB DFU?