Question
Program gets stuck in for loop after interrupt runs
This has me scratching my head - my program runs fine UNLESS the interrupt occurs, after which it gets stuck in a for loop near the start of the program. I can't see any way these two things are connected with each other - there dont share variables. The main loop is as follows
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_ADC1_Init();
MX_SPI1_Init();
MX_TIM1_Init();
MX_TIM2_Init();
MX_TIM16_Init();
ADC12_COMMON ->CCR |= 1<<19 | 1 <<17; // set ADC clock options
ADC1->CR |= 1>>0; // enable ADC
ADC1->CR |= ADC_CR_ADSTART; // start conversion
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_4);
HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1);
while (1)
{
while(((ADC1->ISR) & 0b00000100)==0)
{
}
for(j=0;j<10;j++)
{
ADC_result_pre[i][j] = ADC1->DR; //fetch adc data
}
VCA_raw[i]= (ADC_result_pre[i][0]+ADC_result_pre[i][1]+ADC_result_pre[i][2]+ADC_result_pre[i][3]+ADC_result_pre[i][4]+ADC_result_pre[i][5]+ADC_result_pre[i][6]+ADC_result_pre[i][7]);
ADC_result[i] = VCA_raw[i] / 8;
switch(ADC1->SQR1) //switch dac channel to the next
{
case 0b101000000:
ADC1 ->SQR1 = 0b110000000;
i=1;
break;
case 0b110000000:
ADC1 ->SQR1 = 0b101000000;
i=0;
break;
}
ADC1->CR |= ADC_CR_ADSTART;
//======================================================================
LED1_prep = ADC_result[0]>>4;
RED1 = 255 - LED1_prep;
BLUE1 = LED1_prep;
if(RED1 <= 127)
{
GREEN1 = RED1*2;
}
else
GREEN1 = BLUE1*2;
set_rgb1(RED1,BLUE1,GREEN1); //second spot is actually blue // third is green
LED2_prep = ADC_result[1]>>4;
RED2 = 255 - LED2_prep;
BLUE2 = LED2_prep;
if(RED2 <= 127)
{
GREEN2 = RED2*2;
}
else
GREEN2 = BLUE2*2;
set_rgb2(RED2,BLUE2,GREEN2); //1st green, 2nd red, third blue
//========================================================================
Prepare_States(ADC_result[0],0); //get the mode info for the first channel
prep_values(0);
// dac_channel = 1;
Prepare_States(ADC_result[1],1); //and for the second
// prep_values(1);
}
}It gets stuck on the for loop on line 32. I can see j incrementing up to 9, then it gets reset and stays in the loop. The interrupt is as follows
void EXTI15_10_IRQHandler(void)
{
uint32_t mask = 0;
uint32_t Chuff = ChangeFlag;
if (Chuff & 1<<2)
mask = (1<<4);
else
mask = (1<<20);
if (Chuff & 1<<3)
mask |= (1<<12);
else
mask |= (1<<28);
GPIOA->BSRR = mask;
Chuff |= 1<<0;
ChangeFlag |= Chuff;
EXTI->PR1 |= 1<<11; //turn off interrupt request
}I can't see any way these things are related. Any help much appreciated!