Skip to main content
mcho.19
Associate II
October 23, 2018
Question

Program does not start with my bootloader in some case

  • October 23, 2018
  • 0 replies
  • 475 views

I am making a program with a board made by my company

It is a board using STM32F207

I made a boot loader and decided to jump to 0x08020000 when it started

Then, I made a program and set the vector table to 0x08020000

So the program works well

However, it may not work due to slightly changing programs

I think that it jump to the program normally from the boot loader but hang up immediately after jumping to the program

Just by initializing a variable from a normally working source to a function with memset or the like may cause problems

It is not that it gets strange from the modified place, but the program does not start at all in that one sentence

Modify the vector table of this inoperative program to 0x08000000 and operate normally without boot loader

Debugging is impossible because there is no debugging device

Please help me

This is a part of my program

stm32f207xx_flash.icf

/*-Specials-*/

define symbol __ICFEDIT_intvec_start__ = 0x08020000;

/*-Memory Regions-*/

define symbol __ICFEDIT_region_ROM_start__ = 0x08020000;

define symbol __ICFEDIT_region_ROM_end__  = 0x080FFFFF;

define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;

define symbol __ICFEDIT_region_RAM_end__  = 0x20020000;

/*-Sizes-*/

define symbol __ICFEDIT_size_cstack__ = 0x1000;

define symbol __ICFEDIT_size_heap__ = 0x2000;

system_stm32f2xx.c

in void SystemInit(void)

 SCB->VTOR = 0x08020000;

    This topic has been closed for replies.