Skip to main content
ayaka
Associate II
June 29, 2010
Question

Program chip using st-link in Atollic IDE

  • June 29, 2010
  • 12 replies
  • 2661 views
Posted on June 30, 2010 at 01:19

Program chip using st-link in Atollic IDE

    This topic has been closed for replies.

    12 replies

    hooman14
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:56

    Nope,

    But i used your awesome program to create the binary.

    I fixed my issue.My problem was that BOOT0 pin was floating. once I grounded that pin, my program started running. While it was floating, i had to execute a RUN core command from ST-LINK utility to get it working (which i'm not sure if that part makes any sense...)

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 13:56

    having the same issue aaron, did you find a solution ?

    Does the ST-LINK Utility even support .HEX files? I wrote and posted a ELF to BIN/HEX utility to this (STM32) or the STM32 VL forum a while back.

    But to be honest the eval versions of KEIL or IAR would serve you better.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..