Skip to main content
SHong.5
Associate III
Nov 25, 2020 7:15 AM UTC
Solved

[Procedures] How to use example codes : STM32Cube_FW_H7

Hi

​

I'm currently using STM32H743 and would like to try out example codes from STM32Cube_FW_H7.

​

Desktop\STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_UDP_Echo_Client

​

There were files in above directory.

  • EWARM
  • Inc
  • MDK-ARM
  • Src
  • SW4STM32

​

​Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32.

However, after I BUILD PROJECT, the message "Info: Nothing to build for STM32H743I_EVAL". I tried to import src, inc folders, but it seems like it doesn't compile.

Can anybody help me out with this?

Thanks in advance

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Nov 27, 2020 2:12 AM UTC

> Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32

​

Unfortunately SW4STM32 projects don't build as is with Atollic. You have to import (convert) them. See the Atollic documentation.

After conversion, fix some small issues - if I remember correctly, make the project to use the original linker script (.ld file) instead of auto-created.

-- pa

5 replies

Pavel A.
Pavel A.Best answer
Nov 27, 2020 2:12 AM UTC

> Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32

​

Unfortunately SW4STM32 projects don't build as is with Atollic. You have to import (convert) them. See the Atollic documentation.

After conversion, fix some small issues - if I remember correctly, make the project to use the original linker script (.ld file) instead of auto-created.

-- pa

ST Technical Moderator
Nov 27, 2020 8:07 AM UTC

Hello @SHong.5​ ,

You can use STM32CubeIDE (all-in-one multi-OS development tool) and follow the guide to import Cube projects from SW4STM32 or TrueSTUDIO to STM32CubeIDE:

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Frak.1
Associate II
Nov 27, 2020 8:42 AM UTC

@Imen DAHMEN According to UM2579 that you have linked, it is not possible to convert multicore SW4STM project to CubeIDE.

The guide says:

• It is not possible to convert to STM32CubeIDE a mutlicore project created in System Workbench for STM32

And @SHong.5 is using dualcore STM32H7.

Regards,

ST Technical Moderator
Nov 27, 2020 9:43 AM UTC

Hi @Frak.1​ ,

That sentence is a bit old, the guide is old and probably needs updating.

I recommend you to follow the AN5361 STM32H7 guide for import, in Section 2.5 Import a project from the STM32CubeH7 MCU Package.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks