Skip to main content
TJM
Senior II
May 6, 2020
Question

Procedure for obtaining certificates to use the st-dashboard-iot..... with the IOT Node???

  • May 6, 2020
  • 0 replies
  • 327 views

I put this in Mems and Sensors mainly because I'm using the BL475EIOT (IOT Node) which appears to be a sensor platform.  Since this is new to me and the tutorials that I found have the user bouncing all over the place for information, the questions becomes 'is there a tutorial that will allow this board to connect BOTH to the st-dashboard and to the aws-dashboard? No luck on either, so far. I'm sure I'm missing a piece of information somewhere. Board has v1.4 firmware from the X-aws-cloud expansion pack, configuration of the board for connection to the local access point is successful but appears to be balking at either the server address or some certificate confusion (probably on my part). Looking for a step-by-step procedure/tutorial.

thanks,

tjm

    This topic has been closed for replies.