Skip to main content
beppe2
Associate
November 26, 2009
Question

procedure for enter/exit STOP mode with one EXTI line interrupt

  • November 26, 2009
  • 1 reply
  • 750 views
Posted on November 26, 2009 at 04:49

procedure for enter/exit STOP mode with one EXTI line interrupt

    This topic has been closed for replies.

    1 reply

    beppe2
    beppe2Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:31

    Hi all,

    i am trying to enter and exit STOP mode PWR_EnterSTOPMode within a EXTI line connected to an external button (GPIO).

    The behavior i'd like to have is a single button that when pressed goes into STOP and when pressed again wake up and generate a system reset.

    unfortunately i cannot find a way to make it work, and the posts here do not solve my problems. :(

    with PWR_STOPEntry_WFI, i cannot exit from Stop mode. with PWR_STOPEntry_WFE it goes in hard fault when i press the button the second time to wake it up. could someone explain the basic procedure to make it work?

    here is the relevant code:

    -----------SETUP:

    NVIC_InitTypeDef NVIC_InitStructure;

    EXTI_InitTypeDef EXTI_InitStructure;

    GPIO_InitTypeDef GPIO_InitStructure;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOE, &GPIO_InitStructure);

    GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_PinSource3);

    EXTI_InitStructure.EXTI_Line = EXTI_Line3;

    EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

    EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;

    EXTI_InitStructure.EXTI_LineCmd = ENABLE;

    EXTI_Init(&EXTI_InitStructure);

    NVIC_InitStructure.NVIC_IRQChannel = EXTI3_IRQChannel;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    -----------in ISR:

    void EXTI3_IRQHandler(void)

    {

    EXTI_InitTypeDef EXTI_InitStructure;

    if(EXTI_GetITStatus(EXTI_Line3) != RESET)

    {

    EXTI_ClearITPendingBit(EXTI_Line3);

    GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_PinSource3);

    EXTI_InitStructure.EXTI_Line = EXTI_Line3;

    EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Event;

    EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;

    EXTI_InitStructure.EXTI_LineCmd = ENABLE;

    EXTI_Init(&EXTI_InitStructure);

    PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFE);

    NVIC_GenerateSystemReset();

    }

    what am i missing?

    Thank you!