Skip to main content
PG.9
Associate II
August 24, 2022
Solved

Procedure/document to flash images directly to QSPI flash memory form uboot without using tftp on STM32F691

Greetings!

I am working STM32F691 . I want to flash images to QSPI flash memory without using tftp . Requesting you to kindly help us with procedure/steps for the same.

Thanks in advance

This topic has been closed for replies.
PG.9
PG.9Best answer
Associate II
August 24, 2022

Greetings,

Sorry, It's STM32F69I.

We are customizing image with Linux BSP, so we are using u-boot.

The other means of loading image to board maybe via UART, SD card or any other option.

Yes, we do have SD card implemented. Kindly share us the procedure if you have any to flash via SD card.

We have STM32F69I based EVK, there we are flashing kernel image via TFTP from u-boot.

whereas in this case(custom board) we are not able to make ethernet up in u-boot, since we are unable to load the image.

That was the reason, we are looking for other option to flash the board and load the kernel.

Thanks in advance,

Poornesh.

3 replies

Tesla DeLorean
Guru
August 24, 2022

What's an F691?

Use STM32 Cube Programmer, with an appropriate External Loader for your board and memory device.

Why are you using uboot?

What other means do you have to get an image too the board?

Does you implementation have an SD Card?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PG.9
PG.9AuthorBest answer
Associate II
August 24, 2022

Greetings,

Sorry, It's STM32F69I.

We are customizing image with Linux BSP, so we are using u-boot.

The other means of loading image to board maybe via UART, SD card or any other option.

Yes, we do have SD card implemented. Kindly share us the procedure if you have any to flash via SD card.

We have STM32F69I based EVK, there we are flashing kernel image via TFTP from u-boot.

whereas in this case(custom board) we are not able to make ethernet up in u-boot, since we are unable to load the image.

That was the reason, we are looking for other option to flash the board and load the kernel.

Thanks in advance,

Poornesh.

Tesla DeLorean
Guru
September 6, 2022

STM32F769i-DISCO

​u-boot should have its own command line details for loading and flashing images.

​

P​ushing the initial u-boot load you'd typically use the ST-LINK or System Loader vis STM32 Cube Programmer, as a .BIN or .DFU file

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..