Problems with SPI Tx DMA transfer interrupt when code is located in other place than 0x08000000
Hello.
I work with STM32L433CC and have the own bootloader that is placed at 0x08000000. It starts and jumps to 0x08002000. There is the main application.
It seems that the application works proper. UART Tx with DMA works fine, UART Tx with DMA too and SPI Rx with DMA works proper. But one interrupt makes MCU frozen: SPI Tx with DMA. It's very strange: why do all interrupts work fine but one does not?
When I put the code in 0x08000000 it works fine. All interrupts work proper.
I use SW4STM32.
In STM32L433CCTx_FLASH.ld I have changed to:
/* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8002000, LENGTH = 248K
} In system_stm32l4xx.c I have changed to:
#define VECT_TAB_OFFSET 0x2000 /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */In Run Configuration Menu at Startup Page I have changed the executable offset to 2000.
It seems that I have done everything correctly. But the shifted code doesn't work properly. Why? Where must I search a problem?