Skip to main content
TPien
Visitor II
December 5, 2018
Question

Problems with configuring the FDCAN of the STM32H743ZI

  • December 5, 2018
  • 1 reply
  • 680 views

We have the following situation: We want to use

the FDCAN of the STM32H743ZI with 500 kbit/s. We've got following

configuration parameters for the FDCAN1:

hfdcan1.Instance = FDCAN1;

    hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

    hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

    hfdcan1.Init.AutoRetransmission = DISABLE;

    hfdcan1.Init.TransmitPause = DISABLE;

    hfdcan1.Init.NominalPrescaler = 50;

    hfdcan1.Init.NominalSyncJumpWidth = 1;

    hfdcan1.Init.NominalTimeSeg1 = 13;

    hfdcan1.Init.NominalTimeSeg2 = 2;

    hfdcan1.Init.DataPrescaler = 50;

    hfdcan1.Init.DataSyncJumpWidth = 1;

    hfdcan1.Init.DataTimeSeg1 = 13;

    hfdcan1.Init.DataTimeSeg2 = 2;

    hfdcan1.Init.MessageRAMOffset = 0;

    hfdcan1.Init.StdFiltersNbr = 1;

    hfdcan1.Init.ExtFiltersNbr = 0;

    hfdcan1.Init.RxFifo0ElmtsNbr = 64;

    hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;

    hfdcan1.Init.RxFifo1ElmtsNbr = 64;

    hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;

    hfdcan1.Init.RxBuffersNbr = 64;

    hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;

    hfdcan1.Init.TxEventsNbr = 0;

    hfdcan1.Init.TxBuffersNbr = 2;

    hfdcan1.Init.TxFifoQueueElmtsNbr = 2;

    hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

    hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

    hfdcan1.msgRam.StandardFilterSA = 0x4000AC00;

    hfdcan1.msgRam.ExtendedFilterSA = 0x4000AC40;

    hfdcan1.msgRam.RxFIFO0SA = 0x4000AC80;

    hfdcan1.msgRam.RxFIFO1SA = 0x4000ACC0;

    hfdcan1.msgRam.RxBufferSA = 0x4000AD00;

    hfdcan1.msgRam.TxEventFIFOSA = 0x4000AD40;

    hfdcan1.msgRam.TxBufferSA = 0x4000AD80;

    hfdcan1.msgRam.TxFIFOQSA = 0x4000ADC0;

    hfdcan1.msgRam.TTMemorySA = 0x4000AE00;

    hfdcan1.msgRam.EndAddress = 0x4000D3FF;

    hfdcan1.ErrorCode = 0;

The problem is that Busmaster now only receives Bit and Stuffing errors when we

try to transmit our message frames. We suspect our parameter configuration to mismatch

with Busmaster's baud configuration. Does anyone tested the H7 FDCAN and has experience

in choosing the correct values? Thank you very much.

This topic has been closed for replies.

1 reply

TKrop
Associate II
October 9, 2019

One part that needs configuring that isn't shown here is the clock speed of the FDCAN port, so maybe you missed that. If you are communicating with another ST device, it will work if you set the clock speed of the port and these FDCAN timing parameters to the same values.