Skip to main content
lspr35
Associate II
Dec 7, 2007 3:50 PM UTC
Question

Problems Installing stmcdc.inf

Posted on December 07, 2007 at 16:50

Problems Installing stmcdc.inf

    This topic has been closed for replies.

    3 replies

    lspr35
    lspr35Author
    Associate II
    May 17, 2011 10:18 AM UTC
    Posted on May 17, 2011 at 12:18

    Problem solved:

    After disconnecting and reconnecting the USB cable it was possible to install the driver (for whatever reason...). After that there was an error message in the device status. This could be solved by switching off and on the µC (for whatever reason...).

    Is there a way for an ''easy'' and ''userfriendly'' installation of the driver?

    Regards

    Squonk

    lspr35
    lspr35Author
    Associate II
    May 17, 2011 10:18 AM UTC
    Posted on May 17, 2011 at 12:18

    While trying to test the virtual COM port driver software I encountered the problem, that I can not install the according driver ''stmcdc.inf'' which is provided by ST for this purpose. On two XP systems I receive the error message: ''Der angegebene Ort enthält keine Informationen über die Hardware.''. Sorry I have a german PC! The translation of this error message might be: The given location does not contain information about the hardware''.

    What can I do?

    Best regards

    Squonk

    16-32micros
    Associate III
    May 17, 2011 10:18 AM UTC
    Posted on May 17, 2011 at 12:18

    This prb seems to be known at Microsoft, since it seems that the Native Driver (Usbser.sys) was initially made for Low speed modem some years ago and now is widely used in embedded systems for USB to replace Applications using UART/RS232 to communicate with Embeddeed designs, since few laptops/Desktops are nowadays having the old RS232.

    http://support.microsoft.com/kb/831480/en-us

    http://support.microsoft.com/kb/833680/en-us

    [ This message was edited by: STOne-32 on 07-12-2007 21:28 ]