Skip to main content
NEERAJ GUPTA
Associate III
July 19, 2017
Question

Problems found in STM32F746G-discovery Kit schematics

  • July 19, 2017
  • 3 replies
  • 823 views
Posted on July 19, 2017 at 14:11

Refering to page no 6 in  mb1191.pdf  which is available as STM32F746G-discovery Kit schematic. 

The pin diagram of following two Arduino connector was incorrect, this need correction as follows:

1. CN4 connector has ARD_D5 pin mentioned as PA8 -> this is incorrect.

    ARD_D5 pin should be connected with PI0 as per rest of schematic.

2. CN7 connector has ARD_D10 pin mentioned as PI0 -> this is incorrect.

    ARD_D10 pin should be connected with PA8 as per rest of schematic.

Please! do this correction urgently. Otherwise it will create a lot of confusion regarding the hardware design.

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    July 19, 2017
    Posted on July 19, 2017 at 16:54

    Hello

    GUPTA.NEERAJ

    ,

    Thank you for bringing this issue to our attention.

    You are right,

    I will highlight this typo error to correct it in coming releaseofSTM32F746G-DISCO schematics pack.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Tesla DeLorean
    Guru
    July 19, 2017
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    NEERAJ GUPTA
    Associate III
    July 20, 2017
    Posted on July 20, 2017 at 06:52

    Thanks for acknowledging this.