Skip to main content
yabool2001
Associate III
October 1, 2023
Solved

problem with UART receiving - IDLE low all time

Hi,

I'm developing STM32G031 UARTs using registers and the CMSIS library. I’m using NUCLEO-G031K8 UART2 over an embedded STLINK/V3 on board and UART1 over an external CP210x UAR/USB adapter.  I have a problem receiving data to UART1. No problem to receive data to UART2. Also both UARTs transmissions are working properly. I’m using the same configuration:

 

// USART1_TX = PA9
// USART1_RX = PA10
// USART2_TX = PA2
// USART2_RX = PA3

void my_uart1_conf ( void )
{
	RCC->IOPENR 	|= RCC_IOPENR_GPIOAEN ;		// Activate clock in GPIOA
	GPIOA->MODER 	&= ~GPIO_MODER_MODE9_0 ; 	// Set Alternate Function (AF) for USART1_TX
	GPIOA->MODER 	&= ~GPIO_MODER_MODE10_0 ; 	// Set Alternate Function (AF) for USART1_RX
	GPIOA->AFR[1]	|= GPIO_AFRH_AFSEL9_0 ; 	// AFRH is AFR[1]. Choose AF1
	GPIOA->AFR[1]	|= GPIO_AFRH_AFSEL10_0 ; 	// AFRH is AFR[1]. Choose AF1
	GPIOA->OTYPER	|= GPIO_OTYPER_OT10 ; 		// Choose Open_drain for RX to avoid P-MOS transistors issues
	//GPIOA->PUPDR	|= GPIO_PUPDR_PUPD10_1 ;	// Rx Pull-up
	RCC->IOPENR 	|= RCC_IOPENR_GPIOAEN ;		// Activate clock in GPIOA
	RCC->APBENR2	|= RCC_APBENR2_USART1EN ;
	USART1->BRR 	= (uint16_t) ( 16000000 / 115200 ) ;			// Activate clock for UART
	USART1->CR1 	|= USART_CR1_UE ;
	USART1->CR1 	|= USART_CR1_TE ;
	USART1->CR1 	|= USART_CR1_RE ;
}

void my_uart2_conf ( void )
{
	RCC->IOPENR 	|= RCC_IOPENR_GPIOAEN ;		// Activate clock in GPIOA
	GPIOA->MODER 	&= ~GPIO_MODER_MODE2_0 ; 	// Set Alternate Function (AF) for USART2_TX
	GPIOA->MODER 	&= ~GPIO_MODER_MODE3_0 ; 	// Set Alternate Function (AF) for USART2_RX
	GPIOA->AFR[0]	|= GPIO_AFRL_AFSEL2_0 ; 	// AFRL is AFR[0]. Choose AF1
	GPIOA->AFR[0]	|= GPIO_AFRL_AFSEL3_0 ; 	// AFRL is AFR[0]. Choose AF1
	GPIOA->OTYPER	|= GPIO_OTYPER_OT3 ; 		// Choose Open_drain for RX to avoid P-MOS transistors issues
	RCC->IOPENR 	|= RCC_IOPENR_GPIOAEN ;		// Activate clock in GPIOA
	RCC->APBENR1	|= RCC_APBENR1_USART2EN ;
	USART2->BRR 	= (uint16_t) ( 16000000 / 115200 ) ;			// Activate clock for UART
	USART2->CR1 	|= USART_CR1_UE ;
	USART2->CR1 	|= USART_CR1_TE ;
	USART2->CR1 	|= USART_CR1_RE ;
}

 

In debug mode I verified GPIOA, UART1 and UART2 configuration and all registers’ values are the same. Exception is an ISR. There are following differences on ISRs register after UARTs configuration:

ISR Register

UART1

UART2

CMF

1

0

RXNE

1 (goes 0 after some time)

0

IDLE

0

1

FE

1

0

I tried also:

  • change UART/USB adapter,
  • different mix of UART1 OTYPER and PUPDR configuration,

without success.

 

Do you have an idea what I should change in GPIOA or USART1 configuration to be able to receive data to UART1?

V/r

yabool2001

This topic has been closed for replies.
TDK
TDKBest answer
October 1, 2023

If FE (frame error) is set, that suggests the signal coming in in USART1_RX is invalid. Can you view it on a scope or logic analyzer?

Have you tried the setup in CubeMX and comparing the configuration of USART and GPIO registers?

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
October 1, 2023

If FE (frame error) is set, that suggests the signal coming in in USART1_RX is invalid. Can you view it on a scope or logic analyzer?

Have you tried the setup in CubeMX and comparing the configuration of USART and GPIO registers?

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
yabool2001
Associate III
October 1, 2023

Tried CubeMX setup and differen setting and HAL library without success. But your suggestion to check signal on a scope (I'don't have) goaded me to change pins to PB6-7 and it works! So probably my PA10 pin has been broken.

Thanks for inspiration.