Skip to main content
Cart Raziox 1993
Visitor II
August 21, 2018
Question

Problem with synchronization between STM32F7 Nucleo-F767ZI and OV5642 camera by Omnivision. How setting the external synchronization of the OV5642 and Nucleo-F767ZI?

  • August 21, 2018
  • 0 replies
  • 523 views

I have an issue because the DCMI stay in a busy state and never acquire data from the DCMI. I have configured the camera for a VGA resolution and i want acquire that data through parallel interface using the DCMI and DMA of Nucleo board.

Please, i hope the community can help me with this.:sleeping_face:

This topic has been closed for replies.