Question
problem with stm32g474cet6 - no connection via swd
Hello everyone. I have a homemade board with a stm32g474cet6 processor. I can't connect to the processor via swd, while if boot0 is closed to +3.3v, then the chip is perfectly programmed via uart. I rechecked the board, all the blocking capacitors are installed, the contact from the programmer along the lines of swdio, swclk is, boot0 is connected to the ground. I even tried to solder the chip - the behavior does not change. I tried to connect Hard Reset, Connect under Reset - it does not connect. What am I doing wrong?