Skip to main content
Michael Green
Associate
May 22, 2017
Question

Problem with STM32F769I-DISCO LCD initializing with provided Example

  • May 22, 2017
  • 6 replies
  • 1554 views
Posted on May 22, 2017 at 10:49

Hello,

I recently bought the STM32F769I-DISCO to learn and do independent work with the M7-Cortex MCU series, and decided that the features of this board would be sufficient for such work, having special interest in working with its provided LCD as well.

I'm currently using the Eclipse IDE and have the Cross ARM toolchain installed, using the 2017 q1 version. I was able to build the GPIO example or the Blinky LED and have the board be able to communicate with both LEDs. I decided afterwards to jump straight into the DSI_LCD examples to see how they work. I installed the BSP packages and had everything set up correctly as far as I'm concerned, with the header/source files provided being able to compile correctly. The driver packages by the way were compiled by STM32-CubeMX, and I initialized all peripherals to their default state, as well as enable the LCD and LEDs.

The example is supposed to draw from 2 images, both which are apparently inside the header files stored in the form of a massive array which colors a 320x240 image. Everything compiled nicely, with the exception of some common warnings about unused variables (which if I haven't already mentioned, the source, header and BSP files were provided from the ST 1.7.0 package while the drivers were provided from the CubeMX software). Once that's done, I flash it using ST-LINK 4.0.

The image attached is what appears when the flash is complete. A mess of pixel noise with some odd blocks. I have no idea what the problem could be considering this is supposed to be an example project that, according to the readme, should just work in drawing the images if the drivers were set up correctly. I should mention specifically that this project in question is the LCD_DSI_VideoMode_SingleBuffer provided in the STM32Cube_FW_F7_V1.7.0 package.

Any idea on what to do to fix this would be greatly appreciated!

#support
    This topic has been closed for replies.

    6 replies

    john doe
    Senior III
    May 22, 2017
    Posted on May 22, 2017 at 12:15

    maybe those compiler warnings are trying to tell you something is wrong.

    Michael Green
    Associate
    May 23, 2017
    Posted on May 23, 2017 at 06:09

    I checked the warnings but I'm not seeing anything relevant to why the screen is acting as it is. They're only common warnings, and I've tried using the BSP commands for the LCD and some work, such as turning on or off the display, changing brightness. What doesn't seem to work is setting a layer and attempting to draw a shape of any kind, nor is the example file capable of putting the image like it intended. I tried making a clean main file and initializing the LCD on my own, but just using the LCD_Init function gives me the same problem. It's like turning on the LCD causes it to show this screen. I can't tell if the screen is broken (somehow) or if there's some fundamental thing I'm missing from this example.

    EDIT: There is one observation I forgot to mention. The HAL_Delay() is acting strange, where using a value such as 3000ms causes the delay to actually act in 1500ms. This is weird to me considering the blinking LED project worked fine and accurately when I used HAL_Delay() for it. I'm not sure if this incorrect timing is related to the problems of the screen though.

    john doe
    Senior III
    May 24, 2017
    Posted on May 24, 2017 at 03:31

    why dont you start by importing the example into your ide without any modifications and just try building and running it.  it should build without any warnings and should display the image correctly.

    Michael Green
    Associate
    May 24, 2017
    Posted on May 24, 2017 at 03:53

    I did, I imported the entire example, used the drivers it provided, left all the files as is and it does compile. It still shows warnings though; the warnings only talk about functions not used and how the initializer for 'DrawRGBImage' was missing, which at first I thought was the root of the problem, at least it made sense that it sounded like the problem. The thing is, it's saying there should be an initializer in a read-only file, I'm unsure why I should even have to add it to the typedef struct when it should be working by default anyways.

    Also, the actual main.c file provided doesn't utilize it at all. It uses a custom CopyBuffer function that basically sets up the screen to cycle between two images coded into the header files. When that wasn't working, I got rid of it and decided to just use the BSP functions that came with the BSP package and, while some functions work, anything involving manipulation of the screen's pixels (besides brightness or turning on off the display) doesn't work. I'm at a loss as to whether the LCD really is broken or there's something wrong with the initialization of the LCD.