Skip to main content
kitty7c6
Associate
November 30, 2018
Question

Problem with stm32f745 work

After the firmwared (or power off-on) and after the reset the same program takes a different amount of time in ticks. Find it in my oun code. Then tried to create code in Cube and check it - same thing. Then I checked clocking settings and frequency - it was same and after power off-on and after reset (HSE 8MHz, Sys 216M). Then I checked systic interruption systic (setting for 1ms), and it always was 1ms.

What to do and why it can be?

For example the simplest program:

volatile uint32_t *DWT_CONTROL = (uint32_t *)0xE0001000;

volatile uint32_t *DWT_CYCCNT = (uint32_t *)0xE0001004; 

volatile uint32_t *DEMCR = (uint32_t *)0xE000EDFC; 

volatile unsigned int *DWT_LAR   = (volatile unsigned int *)0xE0001FB0;

uint32_t Mcounter, count;

main()

{

 *DWT_LAR = 0xC5ACCE55; // unlock (CM7)

 // enable the use DWT

*DEMCR = *DEMCR | 0x01000000;

// Reset cycle counter

*DWT_CYCCNT = 0; 

// enable cycle counter

*DWT_CONTROL = *DWT_CONTROL | 1 ;

SystemClock_Config();

while(1)

{

u8 i=0;

Mcounter=*DWT_CYCCNT;

i =1;

count=*DWT_CYCCNT-Mcounter;

float op_time=count/216.0f;// count/F_CPU

SendToUart(count);

}

}

count after power off-on = 0;

count after reset = 34 ticks;

    This topic has been closed for replies.

    10 replies

    kitty7c6
    kitty7c6Author
    Associate
    November 30, 2018

    help...somebody..please

    Tesla DeLorean
    Guru
    November 30, 2018

    where are you?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    kitty7c6
    kitty7c6Author
    Associate
    November 30, 2018

    RU, Siberia and unclear_how_the_code_works

    Tesla DeLorean
    Guru
    November 30, 2018

    What tool chain? What optimization level?

    Have you looked at the generated code?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    November 30, 2018

    Quick test on F746G-DISCO, cleaned code up, but seems not to clock after power cycle

    Hello World!
     5 12
     3 200190208
     3 400390211
     3 600590210
     3 800790208
     3 1000990210
     3 1201190208
     3 1401390212
     3 1601590211
     3 1801790208
     3 2001990208
     0 0 << Stopped Debugging in Keil
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
    Hello World! << Reset Button
     3 11
     3 200190212
     3 400390212
     3 600590215
     3 800790212
     3 1000990215
     3 1201190212
     3 1401390216
     3 1601590215
     3 1801790212
     3 2001990215
     3 2202190212
     3 2402390214
     3 2602590216
     3 2802790215
     3 3002990214
     3 3203190215
     3 3403390216
     3 3603590212
     3 3803790216
    Hello World! << Pulling off power jumper and reinstalling
     0 0
    Hello World!
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0
     0 0

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    kitty7c6
    kitty7c6Author
    Associate
    December 3, 2018

    Problem is solved, I use Icache and ART

    static void SetSysClock(void)

    {

     uint32_t PLLM = 8<< RCC_PLLCFGR_PLLM_Pos;

     uint32_t PLLN = 432 << RCC_PLLCFGR_PLLN_Pos;

     uint32_t PLLP = 0 << RCC_PLLCFGR_PLLP_Pos;

     uint32_t PLLQ = 9 << RCC_PLLCFGR_PLLQ_Pos;

     /* Configure Flash prefetch, Instruction cache, Data cache and wait state */

      

     SCB_EnableICache();

      

     FLASH->ACR |= FLASH_ACR_LATENCY_7WS;  

     FLASH->ACR |= FLASH_ACR_ARTEN;  

     /* Select regulator voltage output Scale 1 mode, EnableOverDriveMode */

     PWR->CR1 |= (PWR_CR1_VOS_0 | PWR_CR1_VOS_1) | PWR_CR1_ODEN;

      

     /* Enable HSE */

     RCC->CR |= ((uint32_t)RCC_CR_HSEON); 

     /* Wait till HSE is ready */

     while((RCC->CR & RCC_CR_HSERDY)!=RCC_CR_HSERDY){} 

      

     /*RCC_PLL_ConfigDomain_SYS*/

     RCC->PLLCFGR &=~ RCC_PLLCFGR_PLLSRC | RCC_PLLCFGR_PLLM | RCC_PLLCFGR_PLLN | RCC_PLLCFGR_PLLP | RCC_PLLCFGR_PLLQ; //clear mask 

     RCC->PLLCFGR = RCC_PLLCFGR_PLLSRC_HSE | PLLM | PLLN | PLLP | PLLQ; //set mask 

     RCC->CR |= RCC_CR_PLLON; 

     /* Wait till PLL is ready */ 

     while((RCC->CR & RCC_CR_PLLRDY) != RCC_CR_PLLRDY){} 

      

     RCC->CFGR &=~ (RCC_CFGR_HPRE | RCC_CFGR_PPRE1 | RCC_CFGR_PPRE2 | RCC_CFGR_SW);

     /*RCC_SetAHBPrescaler HCLK = SYSCLK / 1*/

     /*RCC_SetAPB1Prescaler PCLK2 = HCLK / 4*/

     /*RCC_SetAPB2Prescaler PCLK2 = HCLK / 2*/

     /*RCC_SetSysClkSource*/

     RCC->CFGR |= (RCC_CFGR_HPRE_DIV1 | RCC_CFGR_PPRE1_DIV4 | RCC_CFGR_PPRE2_DIV2 | RCC_CFGR_SW_PLL);

     /* Wait till System clock is ready */

     while((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL) {} 

    }