Skip to main content
161673
Associate
November 28, 2011
Question

Problem with Steval-IFS013V1's DFU example

  • November 28, 2011
  • 2 replies
  • 550 views
Posted on November 28, 2011 at 03:38

The DFU created from hex file, which was built from example project (sink.rprj and sensor.rprj) doesn't work - after upload the DFU in dfu mode and replug the USB dongle isn't identified by system (I tried on Windows and Linux).

The DFU's included in example works - USB dongle is identified (PID 5740). 

1. Why created hex file doesn't work?

2. What I can do to create a working hex file?

I using Ride7 ver. 7.30.10.0159 with 7.30.10.0169 Path, RKit-ARM ver. 1.26.10.0130, DFU file manager v3.0.0 and DfuSe Demo v3.0.0
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 28, 2011
    Posted on November 28, 2011 at 04:17

    One might hazard that the code is not being compiled for the correct address.

    Examining the first couple of lines of each hex file might be quite instructive.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    161673
    161673Author
    Associate
    November 28, 2011
    Posted on November 28, 2011 at 13:35

    I attached the hex file. Can you look at it?

    ________________

    Attachments :

    sensor.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtVj&d=%2Fa%2F0X0000000aR4%2Fr7vqJ6.hb4MJ0Xwm0HerMJbTnVmFqow3fMFkzQW1qGc&asPdf=false