Skip to main content
Associate
July 31, 2024
Solved

Problem with st-flash while programming Nucleo H563ZI

I am using st-flash version of 1.8.0 to flash the binary into Nucleo H563ZI. In this process i have used erase command "st-flash --connect-under-reset erase" to check whether the hardware works or not. For the erase command i got below error
"
st-flash 1.8.0
2024-07-31T16:31:55 WARN common.c: NRST is not connected
2024-07-31T16:31:55 ERROR common.c: Soft reset failed: error write to AIRCR
2024-07-31T16:31:55 ERROR common.c: Can not connect to target. Please use 'connect under reset' and try again
Failed to connect to target
Failed to parse flash type or unrecognized flash type
"
I have also tried with st-link's git upstream master(1.8.0-39-gd7103ff) for testing yet the above error persists. I am using WSL2 on native windows machine.

Does anyone has similarish or related issues for the STM32H563ZI target?

This topic has been closed for replies.
TDK
TDKBest answer
July 31, 2024

It just isn't fully supported yet. This is not an ST application, it's an open source community tool.

stlink/doc/supported_devices.md at testing · stlink-org/stlink (github.com)

If you use official tools, they should work. STM32CubeProgrammer has a command line interface (CLI).

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
July 31, 2024

It just isn't fully supported yet. This is not an ST application, it's an open source community tool.

stlink/doc/supported_devices.md at testing · stlink-org/stlink (github.com)

If you use official tools, they should work. STM32CubeProgrammer has a command line interface (CLI).

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
August 1, 2024

@TDK 

Thank you for the answer.