Skip to main content
erikszah
Associate
September 14, 2008
Question

Problem with SPI1

  • September 14, 2008
  • 4 replies
  • 894 views
Posted on September 14, 2008 at 20:29

Problem with SPI1

    This topic has been closed for replies.

    4 replies

    erikszah
    erikszahAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    Hi,

    I am quite new to STM32 and I have a problem with SPI1. I have 2 boards with stm32 microcontrollers. On one board there is STM32F103RBT6, but on the other board STM32F103R6T6. So the problem. When I try to use SPI1 it doesn't work on both boards but the board with STM32F103RBT6 has 2 SPIs and SPI2 is working fine. That SPI1 stucks in

    while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)==RESET);

    What is the problem?

    My SPI1 configs:

    GPIO_InitTypeDef GPIO_InitStructure;

    SPI_InitTypeDef SPI_InitStructure;

    /* GPIOA and GPIOC Periph clock enable */

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

    /* SPI1 Periph clock enable */

    RCC_APB1PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

    /* Configure SPI1 pins: SCK, MISO and MOSI */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    /* Configure PA4 pin: CS pin */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    /* SPI1 Config */

    SPI_I2S_DeInit(SPI1);

    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

    SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

    SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8;

    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

    SPI_InitStructure.SPI_CRCPolynomial = 7;

    SPI_Init(SPI1, &SPI_InitStructure);

    /* SPI1 enable */

    SPI_Cmd(SPI1, ENABLE);

    Thanks!

    Erik

    erikszah
    erikszahAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    These controllers are from 'Performance line'.

    So what is the solution to this problem? I cannot find any other way to check this flag.

    Erik

    [ This message was edited by: erikszah on 14-09-2008 23:42 ]

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    Both of your devices are, ''medium density'' - these do not support I2S flavor of SPI.

    I note that you are using full-duplex - suggest that you temporarily use a simpler application - to see if you can first get it to work.

    um0427/FWLib/examples/SPI/Simplex_Interrupt/main.c

    Use this code which is simpler and see if this works. Note that you must #define SPI_Mode_Select so that I2S mode is not chosen. Give this a try

    [ This message was edited by: jj.sprague on 14-09-2008 23:57 ]

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:45

    Please try my suggestion (edited in my earlier post). Good luck.