Problem with socket configuration while using MXCHIP Wi-Fi Component
Hi, I have been developing IoT application for the B-U585I-IOT02A (STM32U585AI) and encountered following problem:
When attempting to set a socket to non-blocking mode MX_SO_BLOCKMODE = 1 using the MX_WIFI_Socket_setsockopt() API the call fails immediately and returns -1.
Steps to reproduce:
1. Create a socket using MX_WIFI_Socket_create()
2.Try to configure MX_SO_BLOCKMODE = 1 MX_WIFI_Socket_setsockopt()
3. Get instant -1 in the runtime
Minimal Reproducible Code
#include "mx_wifi.h"
#include "mx_wifi_bare_os.h" /* Using Bare OS mode */
void test_nonblocking_socket_config(void)
{
int32_t sock = -1;
int32_t optval = 1; /* 1 = Non-blocking mode */
int32_t ret = -1;
/* 1. Create TCP Socket */
sock = MX_WIFI_Socket_create(MX_WIFI_AF_INET, MX_WIFI_SOCK_STREAM, MX_WIFI_IPPROTO_TCP);
if (sock < 0)
{
/* Handle socket creation failure */
return;
}
/* 2. Configure Socket to Non-blocking Mode */
ret = MX_WIFI_Socket_setsockopt(sock,
MX_WIFI_SOL_SOCKET,
MX_SO_BLOCKMODE,
&optval,
sizeof(optval));
/* FAILS HERE: ret returns -1 immediately at runtime */
if (ret < 0)
{
/* Socket option rejected by driver/module */
}
}The Wi-Fi link is verified and connected prior to running this code. I am currently using the Bare OS abstraction (mx_wifi_bare_os.h) because CMSIS-RTOS v2 integration (mx_wifi_cmsis_os.h) encountered separate compatibility issues with this setup.
While I am currently working around this issue using standard blocking sockets, non-blocking socket I/O is highly recommended when integrating with the coreMQTT agent library to allow background command loop processing and avoid task starvation.
Has anyone encountered this restriction with MX_SO_BLOCKMODE on the EMW3080 component, or is there an alternative mechanism to achieve non-blocking reads/writes with the stm32 mx wi-fi driver?
WI-FI component: https://github.com/STMicroelectronics/stm32-mx-wifi/tree/main