Skip to main content
bassem.saleh93
Associate II
September 23, 2019
Question

Problem with scanf in STM32F4, it is scanning only the first char even I am requesting to scan an int or float. Details in description

  • September 23, 2019
  • 3 replies
  • 1077 views

here is the code I am using to scan

int ScanConfig(__const char * format, va_list args) {
 unsigned i=0;
 char ch = 0;
 char buffer[256];
 int ret = 0;
 while((i<sizeof(buffer))&&(ch!='\n')&&(ch!='\r')){
 HAL_StatusTypeDef status = HAL_TIMEOUT;
 while (status == HAL_TIMEOUT) {
 status = HAL_UART_Receive(&UartHandle1, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
 if (status == HAL_TIMEOUT) {
 /*HAL_UART_DeInit(&rxHandle);
 HAL_UART_Init(&rxHandle);*/
 }
 else
 break;
 }
 
 buffer[i]=ch;
 i++;
 ret = vsscanf(buffer, format, args);
 if (ret > 0)
 break;
 }
 buffer[i]=0;
 return ret;
}
int Scan(__const char * format, ...) {
 va_list args;
 va_start(args, format);
 int size = ScanConfig(format, args);
 va_end(args);
 return size;
}

I am calling the function like this:

Scan("%f",&InVar);

The problem that if I try to enter 4.5 for example, I can't and it saves only 4.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
September 23, 2019

Which tools/libraries are you using? Are floating point libraries for printf()/scanf() included, or lightweight alternatives?

Do you properly NUL terminate the buffer before calling vsscanf() ? Do you, or should you, clear the buffer[] as it is a local/auto variable holding whatever junk is currently on the stack.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
bassem.saleh93
Associate II
September 23, 2019

I am using HAL library on Eclipse IDE. Yes, floating point is included for printf and scanf. The problem is not that it does print or scan garbage. The problem that it just scans one character.

Tesla DeLorean
Guru
September 23, 2019

Does it actually fill the buffer?

As I already noted you need to NUL terminate the buffer.

Otherwise, perhaps step with the debugger to understand why it is finishing the scan early.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..