Skip to main content
Gregory3
Associate III
Oct 2, 2020 8:09 PM UTC
Solved

Problem with QSPI and external FLASH

Hello!

I'm using a custom board with STM32F767 and external Flash memory connected to the QSPI (MX25L12835F).

I want to create a simple test, where I read and write some data into the external Flash.

In the first shot I want to use the normal SPI mode to:

  1. Readout the Manufacturer & Part ID
  2. Set the Write Enable Bit in the Status Register
  3. Readout the Status Register to check if the Write Enable Bit was set.

So, the first setp (1.) is working fine. I'm getting correct data after reading out the Flash ID.

But when I write to the Status Register and then read out the content, then nothing is changed. My expectation is that the WEL bit will change it's state to 1.

Here the code from the main:

 //Readout the manufacturer and device ID
	sCommand.InstructionMode 	 = QSPI_INSTRUCTION_1_LINE;
	sCommand.Instruction 		 = READ_JEDEC_ID_CMD;
	sCommand.AddressMode 		= QSPI_ADDRESS_NONE;
	sCommand.AlternateByteMode	= QSPI_ALTERNATE_BYTES_NONE;
	sCommand.DataMode			= QSPI_DATA_1_LINE;
	sCommand.DummyCycles		 = 0;
	sCommand.Address			 = 0;
	sCommand.DdrMode			 = QSPI_DDR_MODE_DISABLE;
	sCommand.SIOOMode			= QSPI_SIOO_INST_EVERY_CMD;
	sCommand.NbData				= 3;
 HAL_QSPI_Command(&hqspi, &sCommand, 1000);
 HAL_QSPI_Receive(&hqspi, ID_REG, 1000);
 
 //Set the write enable bit
	sCommand.InstructionMode 	 = QSPI_INSTRUCTION_1_LINE;
	sCommand.Instruction 		 = WRITE_ENABLE_CMD;
	sCommand.AddressMode 		= QSPI_ADDRESS_NONE;
	sCommand.AlternateByteMode	= QSPI_ALTERNATE_BYTES_NONE;
	sCommand.DataMode			= QSPI_DATA_1_LINE;
	sCommand.DummyCycles		 = 0;
	sCommand.Address			 = 0;
	sCommand.DdrMode			 = QSPI_DDR_MODE_DISABLE;
	sCommand.SIOOMode			= QSPI_SIOO_INST_EVERY_CMD;
	sCommand.NbData				= 0;
 HAL_QSPI_Command(&hqspi, &sCommand, 1000);
 HAL_Delay(200);
 //From now on the ext. FLASH will accept write commands
 
 //Readout the status register
	sCommand.InstructionMode 	 = QSPI_INSTRUCTION_1_LINE;
	sCommand.Instruction 		 = READ_STATUS_REG_CMD;
	sCommand.AddressMode 		= QSPI_ADDRESS_NONE;
	sCommand.AlternateByteMode	= QSPI_ALTERNATE_BYTES_NONE;
	sCommand.DataMode			= QSPI_DATA_1_LINE;
	sCommand.DummyCycles		 = 0;
	sCommand.Address			 = 0;
	sCommand.DdrMode			 = QSPI_DDR_MODE_DISABLE;
	sCommand.SIOOMode			= QSPI_SIOO_INST_EVERY_CMD;
	sCommand.NbData				= 1;
 HAL_QSPI_Command(&hqspi, &sCommand, 1000);
 HAL_QSPI_Receive(&hqspi, Status_Reg, 1000);

So the Status_Reg never changes from the initialized state 0.

Thank you for any hint!

Regards,

Gregor

This topic has been closed for replies.
Gregory3
Gregory3Best answer
Associate III
Oct 3, 2020 9:24 PM UTC

Ok, now I solved the problem.

It was this line in the code for the Write Enable Command:

	sCommand.DataMode			= QSPI_DATA_1_LINE;

If the command shall be sent without any "empty" bytes, then this shall be changed to:

	sCommand.DataMode			= QSPI_DATA_NONE;

No it works.

Regards!

5 replies

underpickled
Associate
Oct 2, 2020 8:13 PM UTC

I'm having a very similar problem. I wonder if you can see if we're seeing the same issue. When I put a logic analyzer on the spi lines, I see a transmission of the write enable command (0x06) followed by an extra byte of 0x00 before the CS line goes high. I believe this extra byte is causing the command to fail. I'm on an STM32L452.

Gregory3
Gregory3Author
Associate III
Oct 3, 2020 5:32 PM UTC

Ok, I will connect a scope to the ext Flash and check if the additional byte will be sent. I will let you know.

Oct 3, 2020 3:24 AM UTC
Gregory3
Gregory3AuthorBest answer
Associate III
Oct 3, 2020 9:24 PM UTC

Ok, now I solved the problem.

It was this line in the code for the Write Enable Command:

	sCommand.DataMode			= QSPI_DATA_1_LINE;

If the command shall be sent without any "empty" bytes, then this shall be changed to:

	sCommand.DataMode			= QSPI_DATA_NONE;

No it works.

Regards!

underpickled
Associate
Oct 4, 2020 2:17 AM UTC

My command is already set up that way... Very strange. I'm glad your issue is resolved though.​