PROBLEM WITH PERIPHERAL POST-INCREMENT USING DMA - STM32F100VC
Hi,
I am using DMA to transfer the conversion of two injected channels of the ADC module (registers ADC1_JDR1 & ADC1_JDR2) to a buffer in ram. The conversion is started by software (JSWSTART).
Since the transfer is for two consecutive records, I have set the following configuration:
DMA1_CCR1:
MINC = 1
PINC = 1
DIR = 0
EN = 1
DMA1_CNDTR1 = 2
DMA1_CPAR1 = &ADC1_JDR1
DMA1 _CMAR1 = &buffer_ram
Unexpectedly only the record ADC1_JDR1 is transferred, although Number of Data Transfer is 2.
Only for test purposes I have changed PINC = 0 and then the record ADC1_JDR1 is transferred 2 times, as expected.
What is wrong ??