Skip to main content
naserghasemi2012
Associate II
February 7, 2016
Question

problem with interrupts (stm32f103re)

  • February 7, 2016
  • 1 reply
  • 576 views
Posted on February 07, 2016 at 09:54

Hi

I configured 2 EXTI (PA0 & PB1 ) and work perfectly. But when I configure Port B pins output and connect a led to them ( or even a wire!) inerrupts occure! (I pulled up intrnally and externally PA0 & PB1 and in port B I used SPI)

 can any one help me to use other pins of port B?
    This topic has been closed for replies.

    1 reply

    pkumar1883
    Associate III
    February 8, 2016
    Posted on February 08, 2016 at 10:43

    Bit confusing.Try to see on CRO if some noise is coming on GPIO, or send your piece of code.

    /*Please

     mark helpfull

     if this post helps you or solves your problem.*/

    /**disclaimer**/

    /* I am not a person from ST Technical Support Team. So please verify/test any support/suggestion at your end.*/

    /* This post is only for general support purpose and free of any charge.If you need any personal support for your work please contact at 

    embeddeddesign.help@gmail.com

    */