Skip to main content
Arrhenius
Associate III
September 27, 2022
Question

Problem with CLASSB STL_ClockStartUpTest

  • September 27, 2022
  • 0 replies
  • 538 views

Hi,

  • In the snippet below, comment says select PLL as system clock but in code it is configured as HSE clock which one shall be considered?

  /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 

    clocks dividers */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;

  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

  • In CLASSB package 2.3.0, the startup self test is getting failed during cross reference measurement. In the implementation the HAL driver is replaced by custom drivers, whose source is attached in the thread.

Controller: STM32H723ZG

Package: X-CUBE-CLASSB 2.3.0

This topic has been closed for replies.