Skip to main content
litus0801
Associate III
March 24, 2010
Question

Problem with assert_param

  • March 24, 2010
  • 19 replies
  • 4513 views
Posted on March 24, 2010 at 20:39

Problem with assert_param

    This topic has been closed for replies.

    19 replies

    litus0801
    litus0801Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    That was what I did but the error still persist... 

    I don't know what more can I do...

    I tried defining

    DEBUG

    instead of

    USE_FULL_ASSERT

    as you suggested and I also tried to define it in C/C++ compiler macros but no way...

    Why you said ''like in good old library 2.0''? 3.2.0 is not a good one?

    Thanks for replying edison!

    Anyone can suggest something? I'm really lost...

    Tomas DRESLER
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    Change the #ifdef USE_FULL_ASSERT to #ifdef DEBUG, like in good old library 2.0, or simply #define USE_FULL_ASSERT yourself or put USE_FULL_ASSERT in the C/C++ preprocessor macro definitions.

    litus0801
    litus0801Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    Hi again,

    Ok, I did what Neil said and now I can view the preprocessor files (.i). What should I check? How can I know if a macro is working properly?

    Thanks!!

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    This is where it pays to understand how the whole preprocessor-compiler-linker process works.

    If the Linker is giving you this error, it means that the Compiler has generated calls to assert_param as if it were a function.

    This means that your macro definition is not working properly!

    To sort out preprocessor problems like this, find out (in the Compiler Manual) how to view the preprocessor output...
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    litus0801
    litus0801Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    Ooooook!!!

    Thanks, Neil. I think I am still a noob on C programming. Ok, now I know what the problem exactly is. I can see

    assert_param

    in the preprocessor files so that means whant Neil said, the macro ''is not working''. Now the problem is how to fix it. 

    I'm going to find whether it is possible to disable/enable macros in EWARM. Maybe is a configuration parameter I forgot... Any other idea?

    Thanks again Neil!

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    ''How can I know if a macro is working properly?''

     

     

    You do understand what macros are supposed to do, don't you?

    So, if they do that, then we say that they are ''working'' !!

    ;)

     

     

    To recap, a macro is a text substitution - so, instead of seeing ''assert_param'' in the pre-processed text, you should see its expansion.

    If you are still seeing ''assert_param'' in the pre-processed text, then the preprocessor has not expanded it; ie, it has not worked as a macro!
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    Note that there is also a #else which should create a ''null'' definition when USE_FULL_ASSERT is not defined.

    The fact that you're getting neither the ''full'' definition nor the ''null'' definition - so that the compiler thinks it's a function call - suggests that you are not actually including this at all...
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    ''I think I am still a noob on C programming''

     

     

    Note that this is standard 'C' stuff - nothing specifically to do with STM32, IAR, or embedded.

    Therefore any 'C' textbook should help...

    ''I'm going to find whether it is possible to disable/enable macros in EWARM.''

    No, that is not the correct approach!

    What you need to do is to find out how to correctly configure your Project so that the macro works!

    Note that the macro definition is contained within

    #ifdef  USE_FULL_ASSERT

    This means that the definition is effective only if the symbol USE_FULL_ASSERT is defined...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    ''The compiler return first error''

     

     

    What error, precisely, is that?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    litus0801
    litus0801Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:44

    What I did now is that:

    /* Exported macro ------------------------------------------------------------*/

    #ifdef  USE_FULL_ASSERT

      #define assert_param(expr) ((expr) ? (void)0 : assert_failed((uint8_t *)__FILE__, __LINE__))

    #error ----------------------------------------------------- assert full def.

    /* Exported functions ------------------------------------------------------- */

      void assert_failed(uint8_t* file, uint32_t line);

    #else

      #define assert_param(expr) ((void)0)

    #error ----------------------------------------------------- assert null def.

    #endif /* USE_FULL_ASSERT */

    The compiler return first error, so that means that I am including it (maybe I'm wrong?) 

    Thaaaaaanks!!